RECOM once more shows its development expertise by introducing medical-grade DC/DC modules which offer 3.5W, 5W and 6W. These converters offer all key...
The market is flooded with not only cheap, but also illegal copies of electronic components from counterfeiters around the world. Saving a few cents...
RECOM’s recently released REC15E-Z series of 15W isolated DC/DC converters features wide input ranges at low cost in the popular 1”x1” case size. This...
The latest addition to RECOM’s railway portfolio are two 40W and 60W DC/DC converter series in quarter-brick packages with an ultra-wide input voltage...
Steve Roberts publishes his brand new AC/DC Book of Knowledge just in time for electronica 2018. The Technical Director at RECOM is proud to share his...
For its recently released RPM and RBB10 series, RECOM introduces corresponding evaluation boards which offer a shortcut to the otherwise long-winded...
RECOM extends the output options for its latest 15W and 20W AC/DC power supplies. The complete range of single output (5 - 48VDC), dual output options...