Skip to main content

RECOM products are now RoHS2.1 certified

The RoHS Directive was updated under a new EU Directive 2011/65/EU and is now part of the CE marking requirement. Therefore, since January 2013, all CE-marked products must include RoHS2 in their Declaration of Conformity. In 2015, the EC published a recast (RoHS2.1) proposing four additional Pthalate substances (DEHP, BBP, DBP and DIBP). Member States have until 2019 (2021 for medical products) to amend their national laws to comply. RECOM is aware of this publication and introduction date and has already started the re-qualification process.

The only certain way to prove that products are fully RoHS2.1 compliant is to do a full chemical analysis. Therefore, we have started the RoHS2.1 re-certification process to include DEHP, BBP, DBP and DIBP in our RoHS test reports.  We will re-test the remaining industrial and medical products in our portfolio so that we can offer certified DEHP, BBP, DBP and DIBP-free RECOM products in good time for our customers, well before the date of introduction. So far, we have not discovered any of these new restricted substances in quantities that exceed the proposed limits in any of the products tested, so there should be no need for customers to change their part numbers, BOM or stock.

RoHS (Restriction of Hazardous Substances) is not to be confused with REACH (Registration, Evaluation and Authorisation of CHemicals). The RoHS directive is designed to protect the environment from hazardous chemicals in products and the banned substances are strictly limited to less than 0.1% by weight (0.01% for Cadmium) in the affected products. By comparison, the  REACH SVHC list (Substances of Very High Concern) contains many more chemicals, most of which are known or suspected to cause cancer or birth defects if absorbed in high quantities. So REACH is more to protect the workers manufacturing the products than the end user. The other differences are that REACH also applies to chemicals in their pure form (not part of a product) and, despite the risks, small quantities are still allowed to be present in products. RECOM’s products also conform to the REACH regulation as RECOM doesn’t use chemicals in large quantities, either in the manufacturing or end product.

Click here to see the RoHS2 Declaration of Conformity valid for all our standard products.

Solder profile

Our recommended solder profiles can be downloaded by following the link below. For the Reflow Process, we have used the JEDEC-STD020C guidelines (for prefabricated parts with >2,5mm thickness and volumes of 350 - 2000mm³):
RoHS-compliant Solder profile

Through hole Converters (Wave Soldering)

Wave Peak Temperature: 260°C
Max. Contact with the Solder Wave: 255 °C for max. 5 seconds
Pin Flashing: 100% Sn

SMD Converter (Reflow Soldering)

Reflow Peak Temperature: 245 °C for max. 30 seconds
Pin Flashing: SnAgCu

Logo used on the case and packaging to indicate RoHS products

Our RoHS compliant products are labelled in all of our financial documentation (Order Confirmation, Delivery Note and Invoice) with the comment "RoHS-konform" or "RoHS-compliant" next to the article description.

The converters themselves carry the RoHS-compliant symbol (the letters Pb crossed out inside a circle). Additionally, the packaging tubes will carry this symbol as a sticker.